Default Categories, Groups and Properties
The following table includes the default categories, groups and properties defined in the ERP and Route Editor applications:
Category | Group | Property |
---|---|---|
ERP App | Material Import |
|
ERP App | MaterialLot Import |
|
Route App | WorkOrder Import | No default properties |
ERP App | BomItem Import | No default properties |
Process Order App | ProcessOrder Import | No default properties |
Receiving Inspection App | Additional Properties | No default properties |
Non-Conformance App | Approval Workflow |
|
Non-Conformance App | Failed Criteria |
|
The above properties can be used in the respective applications to store, process, and analyze data.
Example: The value of the unitofmeasure property is set by the ERP import for materials.
OP_Threshold is over production threshold. UP_Threshold is under production threshold. The default float value 0.2 represents a threshold of 20%.
Example: Suppose, the planned quantity for a lot is 5. 20% OP_Threshold of 5 calculates the maximum quantity (more than 5) you can add to the lot. 20% UP_Threshold of 5 calculates the minimum quantity (less than 5) you can record and complete the lot.
You can also create more property definitions in the aforementioned groups as required.
Example: When you import a material, if you require more information on the material, you can add more property definitions in the Material Import group to capture and utilize that information. Refer to Create a Property Definition.