About Work Orders, Operations, and Serials/Lots
A work order is a request to manufacture a certain quantity of products. It contains information on the model, route, and quantity of a product that must be manufactured. Work orders are either created in Route Editor or imported into Plant Applications using the Enterprise Resource Planning (ERP) scheduler and import services.
Work orders are grouped by product and are assigned to a specific production line for manufacturing.
A work order comprises the job details and operations. To manufacture each type of product, a sequence of tasks must be performed. Each task or a set of tasks is called an operation. An operation in a work order is an executable job performed on a Production Unit of a Production Line. Operations can be defined either in the route using the Route Editor module or in the work order that you import from an ERP system.
The quantity of the product to be manufactured determines the number of serial numbers that are created.
Work Orders, Operations, and Sequence Numbers in a Motor Manufacturing Unit
- 3 motors of model A
- 2 motors of model B
Work Order Number | Work Order Description | Operations | Serial Numbers |
---|---|---|---|
W.O 1 | To manufacture motors of model A |
|
|
W.O 2 | To manufacture motors of model B |
|
|
Work Order Number | Operation | Serial Number |
---|---|---|
W.O 1 | Shell turning | W.O.1_S1 |
W.O 1 | Shell turning | W.O.1_S2 |
W.O 1 | Shell turning | W.O.1_S3 |
W.O 2 | Shell turning | W.O.2_S1 |
W.O 2 | Shell turning | W.O.2_S2 |
Suppose Operator 2 wants to work on the rotor assembling operation. When Operator 2 logs in to the application, Work Queue displays the rotor assembling operation only after the shell turning operation has been completed for at least one serial number.