Configure iFIX for Alarms
When using the iFIX HMI/SCADA system as your data source, follow this quick walkthrough to successfully get data and alarms flowing for the first time into Operations Hub.
Before you begin
Procedure
- Start the iFIX application.
- Log in to iFIX with a default/guest account.
-
Go to Applications > Security > Security Configuration Utility.
Security is available in the System & Security group.
- On the Security toolbox, select User Account.
-
Select Add to create a user account.
The User Profile dialog appears.
-
Provide iFIX security for the user account:
Field Description Full name Enter a name for the new user account. Login name Enter a login name for the user account. Password Enter a password for the user account. Group Membership Select Modify to add any/all available groups to the user account, then select OK. Security Areas Select Modify to add any/all security areas to the user account, then select OK. Application Features Select Modify to add any/all application features to the user account, then select OK. -
Select OK to save the user profile.
The Password Confirmation dialog appears.
-
Enter the password again and select OK.
The user account is saved with the credentials and added to the Current Users list.
- On the Security toolbox, select Configuration and select Enabled.
-
Go to Applications > OPC UA Configuration.
The iFIX OPC UA Server Configuration Tool screen appears.
- On the Server tab, select the check box for Server Enabled.
- On the Alarms tab, select the check box for Alarms Enabled.
- Select Save and Exit to save the selections, and close the screen.
-
Go to Applications > Database Manager.
The iFIX Database Manager spreadsheet appears.
- Open an existing database, or select Create New on the spreadsheet toolbar to save a new database.
-
On the spreadsheet toolbar, select Add to add blocks to
your database.
The Select a block type screen appears.
-
Select any block type, then select OK.
The selected block type screen appears.
-
On the Basic tab:
- Enter Tag Name.
- Enter I/O Address.
- Select Save.
-
On the Alarm tab:
- Select the check box for Enable Alarming.
-
In the Alarm Options table, enter the alarm
values.
For example:
High High 60 High 40 Low 20 Low Low 10 - Select Save.
-
On the Advanced tab:
- Select the check box for Enable Output.
- Select Save.
The tag name configured with an alarm is added to the spreadsheet. - Repeat steps 8-12 to add more blocks to your database.
What to do next
- Create a data source with OPC UA configuration in Operations Hub.
- Use the alarm card and alarm count widgets in your application.
- Acknowledge Alarms.
- Apply Filters to View Alarms.
- Configure CIMPLICITY for Alarms.