When using the CIMPLICITY HMI/SCADA system as your data source, follow this quick walkthrough to successfully get
data and alarms flowing for the first time into Operations Hub.
Procedure
-
Start the CIMPLICITY Workbench application.
-
From the Workbench toolbar, go to .
The Create User for New Project dialog
appears.
-
Provide these details for the new user account:
Note: You will use the credentials to establish a secure connection with
authentication for the CIMPLICITY data source in Operations Hub.
-
Select Next.
The Create As dialog appears.
-
Enter the name and location for the new project.
Note: For write operations to work, the project name and the CIMPLICITY data
source name in Operations Hub should be the same.
-
Select product options and protocols that will be included in the
project.
-
Select Create.
-
After creating the project, go to .
The Project Properties screen appears.
-
On the OPC UA Server tab, perform these steps.
-
Select the check box for Enable Server.
-
Select Security Configuration, then select the
check box for all the security options you want to enable for the OPC UA
server.
-
On the Operations Hub tab, perform these steps.
-
Provide the following details:
-
Select the check box for Require trusted
connection.
-
If
(Not Trusted)
, go to the CIMPLICITY project's
\data\WebHMIpki\server_certs
folder and copy the
root certificates.
-
Paste the copied certificates in the CIMPLICITY project's
\data\WebHMIpki\trusted_issuers
folder.
-
On the Operations Hub tab, select Test
Connection.
A success message appears updating the connection status as
(Trusted)
.
-
From the CIMPLICITY Workbench project directory, right-click , to create a new device point.
-
Provide the following information for the new point and select
OK.
The Point Properties screen appears.
-
On the Virtual tab, provide these details:
-
On the Alarm tab, provide these details:
-
Select OK to save and close the Point
Properties screen.
-
Repeat steps 6-10 to create more device points.
-
Run the CIMPLICITY project.