Breadcrumb
With the GEBreadcrumb plugin, you can navigate through the asset model.
The purpose of a breadcrumb is to allow you to access an asset's information located anywhere in the asset model hierarchy. A breadcrumb navigation also defines the relationship between different assets in a model.
The breadcrumb navigation is available for all the widgets in Operations Hub. You can navigate in the trend card using breadcrumb.
To use the plugin in the page designer, drag from
to a container in the page.You must specify these breadcrumb properties:
Item | Description |
---|---|
Source Asset Context | Select the source (asset name) for an asset context. The selected
context appears as a default breadcrumb view in the end application. This
asset name must exist in your asset model. |
Target Asset Context | Select the target for an asset context. This target defines where that
output goes on selecting an asset in a breadcrumb, so that it can be fed
either to a query or a global. |
Target Extension Query for Asset Context Properties | Select the target for an extension query. This is a formatted string
with a list of properties that defines the hierarchy of the breadcrumb in
the end application. For example, consider these crumbs in a hierarchy -
first is ???pump???, second is ???pump pressure???, ???pump frequency???, ???pump
vibration???, or ???pump flow???. |
The breadcrumb is customizable, enabling you to add conditions for display navigation. Refer to Page Components for common widget properties.