Mimic Card
A mimic card provides a specific view of a process diagram associated with an asset. This allows you to monitor and control production equipment and processes.
The mimic card widget is available under designing application pages, drag and drop to a container.
. WhenThe mimic card also allows you to update values during runtime, and get results immediately.
Property | Description |
---|---|
Asset Name (Optional Override) | Provide the asset name for which you want to replace its currently
assigned mimic. Note: You can opt to override either an asset name or a
mimic name. If you attempt to override both, only the asset name is
considered. |
Mimic Name (Optional Override) | Provide the mimic name to replace the currently assigned mimic. The
new mimic must use only direct tags (not model-based) for its data
sources. Also, the new mimic cannot use click-target navigation as the
mimic has no context for navigation when loaded in this manner. Note: If
you do not specify an override for both the asset name or mimic name,
then the mimic from the selected asset context in a breadcrumb is
considered. When not using the breadcrumb in an application, it is
mandatory to provide an override either for the asset name or the
mimic name. |
Height | Allows to set the height of the widget at runtime. You can set the values in percent or pixels. For example, 100%, 50%, 300, etc. |