Configure CIMPLICITY Options

Set up CIMPLICITY options to ensure that sessions are properly created.

  1. On the CIMPLICITY/WebSpace node open CIMPLICITY Options.
  2. Select the Webspace tab.
  3. On the left pane, select General.
  4. Select the check box for Autostart Webspace Session Manager.
  5. Verify the port is 4957, then select Apply.


    A message appears to restart the Webspace Session Manager service.
  6. Select Yes to restart the service.
  7. On the left pane, select Server.


  8. Provide these details:
    Field Description
    Windows Server Credentials
    1. Enter a valid User name and Password for the Webspace system.
      Note: The user must be authorized to launch CimView.exe, as well as access the screens directory for the screens that are accessed via the Webspace widget.
    2. Select Test. If successful,
      • Trust UAA appears as Untrusted
      • Generate UAA Client appears as Not generated
    Operations Hub UAA/OAuth2 Setup
    1. Enter the Server URL for the Operations Hub server. For example, https://opshubsystem:443/uaa.
    2. Test for a successful connection.
    3. Select Trust UAA to change its status from untrusted to trusted.
      Note: When trusted, the UAA certificates are copied to the <CIMPLICITY installation>\webspace-session-manager\pki\trusted directory.
    4. Select Generate UAA Client to enter the credentials for UAA Administrator.
      1. Client Id: admin
      2. Client Secret: Enter the Operations Hub secret, which was entered during installing Operations Hub.
      3. Select Generate.

      The status changes to Generated on successful generation of the UAA Client.

    Single/Relay Server Provide the session manager credentials, and select Apply.
    • WSM Admin User: Enter a user name (example: Administrator)
    • Admin Password: Enter a password (example: pass1234)
    • Confirm Password: Enter the same password to confirm.
    Note: This can be any user name/password and does not have to match any specific windows user name or password.
    A message appears to restart the Webspace Session Manager service.
  9. Select Yes to restart the service.