Batch Widgets Overview
This topic describes the widgets used for batch processing.
Within Operations Hub, the batch widgets provide the same functionality as Proficy Batch Execution thick client. Also refer to Set up Batch. The batch widgets use their own data source.
The batch widgets are available under designing application pages, drag-and-drop the respective batch widget to a container and configure its properties.
. WhenProperty | Description |
---|---|
Style Theme | Select either Light or Dark display theme for all the batch widgets across the application. Do not mix and match themes. |
API Base URL | Enter the REST API base URL you want to access. |
Data Source | Select the batch data source. |
Source > Batch Serial Number | Configure the properties to these global variables.
The global parameter values contain batch instance information to execute batch related operations. Global variable can be a string or a number. ![]() |
Source > Procedure ID | |
Source > API Batch ID | |
Source > Batch Id | |
Source > Step Id | |
Source > Recipe ID | |
Target > Selected Batch Serial Number | |
Target > Selected Batch ID | |
Target > Selected Batch Description | |
Target > Selected Recipe ID | |
Target > Selected Recipe Version | |
Target > Selected Step | |
Target > Selected Batch SFC Branch | |
Target > Selected Batch Procedure ID | |
Enable hide columns | Select/Clear the check box to hide/show columns at runtime. |
Request Interval (Seconds) | At runtime, the widget is updated with new information in the set amount of time in seconds. |
eSignature Requirement | By default, e-Signatures are turned off for batch widgets, which is
None . To enable e-Signatures, select any of the
following options:
Note: To e-sign and verify, user/s should be part of the Windows domain
group on the Batch system. e-Signature is available for Batch Control, Batch Step Control, Batch Parameter, Batch Phase Control, Batch Prompts, and Batch Binding Prompts. This is an example of an e-sign
user name and password request at runtime: ![]() |