Batch Phase Control

Allows to individually execute a phase in a batch process.

To set up the batch phase control page in Operations Hub designer:
  1. In the main container, drag-and-drop Batch Menu and Batch Phase Control.
  2. Configure properties for all the widgets added to the phase control page.

At runtime,

  1. Select the Active Phases tab.
  2. Select a Unit and Phase.
  3. Select Acquire Phase.

  4. After acquiring the phase, select a Command to execute from the available commands for the phase.

    The commands are based on the status of the acquired phase.

  5. Enter the batch ID for the phase and select OK.

    Go to Batch List tab to verify that the phase is executed.