SRS Projects

About SRS Project

Creation of an SRS Project allows the user to select one or many of the SRS templates. Once the user has made the selection of templates, a copy of the collection of templates will be made.

The user can link the SRS Project to zero or many of the following elements:

  • SIL Analysis
  • Logic Solver
  • Instrumented Function
  • Protective Loop

The linkage takes place in the context of a linkable item (for example, instrumented function) where the user can search and select an approved SRS Project.

Access an SRS Project

Procedure

  1. Access the SIS Management Overview page.
  2. Select the SRS tab.

    The SRS section appears, displaying a list of SRS Projects.

  3. In the SRS Project Id column, select the SRS Project that you want to access.

    The SRS Project page appears, displaying the Project Summary workspace for the selected SRS Project. The Definition tab is selected by default.

    Note: As needed, you can modify the values in the available fields, and then select to save your changes.

Create an SRS Project

Before You Begin

Procedure

  1. Access the SIS Management Overview page.
  2. In the workspace, select the SRS tab.

    The SRS section appears, displaying a list of SRS Projects.

  3. In the upper-left corner of the SRS section, select .

    The SIS Management page appears, displaying the Project Summary workspace for the SRS Project.

  4. Enter values in the Project ID and Project Description boxes for the new SRS Project, and then select . The Project ID is a required field.

    A confirmation message appears, indicating that the datasheet has been saved successfully.

Results

  • The SRS Project that you created appears in the SRS section of the SIS Management Overview page.

What To Do Next

Access the List of Linked Records in an SRS Project

Procedure

  1. Access the SRS Project for which you want to view the list of linked records.

    The SRS Project page appears, displaying the Project Summary workspace for the selected SRS Project. The following tabs appear in the workspace:

    • Definition: Contains the datasheet for the SRS Project. This tab is selected by default.
    • Instrumented Functions: Contains a list of Instrumented Functions that are associated with the SRS Project.
    • SIL Analysis: Contains a list of SIL Analyses that are associated with the SRS Project.
    • Protective Loop: Contains a list of Protective Loops that are associated with the SRS Project.
    • Logic Solvers: Contains a list of Logic Solvers that are associated with the SRS Project.

  2. Select the tab containing the records that you want to view.
    The SIL Analysis section appears, which contains the list of SIL Analyses that are associated with the SRS Project.

Change the State of an SRS Project

Procedure

  1. Access the SRS Project for which you want change the state.
  2. In the upper-right corner of the workspace, select the button that indicates the current state of the SRS Project. For example, if the current state of the project is In Progress, select In Progress.

    A menu appears, displaying the list of operations that you can perform on the SRS Project to change its state.

  3. Select the necessary operation that will change the state of the project, and then select Done. For example, if you want to change the state of the analysis from Planning to Active, select Begin , and then select Done.
    Note: You can view the states assigned to various users by selecting the Manage State Assignments link. If not already done, you can assign the next state to the appropriate user, and then select Done.

    The state of the SRS Project is changed.

Results

  • Based on the state of the SRS Project, the datasheet is either enabled or disabled for modification:
    • If the state of the SRS Project is changed to Pending Review, the datasheet is disabled.
    • If the state of the SRS Project is changed to In Progress, the datasheet is enabled.
    • If the state of the SRS Project is changed to Pending Review, the datasheet is disabled.
    • If the state of the SRS Project is changed to Approved, the datasheet is disabled. At this stage, the revision number is incremented.

Change the SRS Template that is Defined for an SRS Category in an SRS Project

Procedure

  1. Access the SRS Project for which you want to change the template used in an SRS Category.
  2. In the left pane, select the SRS Category in which the SRS Template needs to be changed.

    The SRS Category page appears.

  3. In the upper-right corner of the workspace, select Change Template.

    The Create new SRS category window appears, displaying a list of available SRS templates.

  4. Select the <SRS Template> radio button, and then select OK.

    The new SRS template is added to the list of SRS categories displayed in the left pane of the <SRS Project> page.

Compare the Revision Records of an SRS Project

Procedure

  1. Access the revision history of the SRS Project.
  2. Select the revision record which you want to compare with the previous revision record.

    The Revision History page displays the details of the selected revision record.

  3. In the upper-right corner of the workspace, select Show Changes.

    The Changes For Selected Datasheet page appears, displaying the comparison details.

Download an SRS Project Report

Procedure

  1. Access the SRS Project for which you want to print an SRS Project report.
  2. On the upper-right corner of the page, select .

    The Save As window appears.

  3. Navigate to the location where you want to save the report, and then select Save.

    The report is downloaded and saved as a .pdf file.

    Note: The actions required in steps 2 and 3 may differ slightly depending on the browser that you use and the browser settings.

Delete an SRS Project

Procedure

  1. Access the SIS Management Overview page.
  2. In the workspace, select the SRS tab.

    The SRS section appears, displaying a list of SRS Projects.

  3. Select the row that contains the SRS Project that you want to delete.
  4. In the upper-right corner of the section, select .
    Note: SRS Projects that are in the Approved state cannot be deleted.

    A confirmation message appears, asking if you really want to delete the SRS Project(s).

  5. Select OK.

    The SRS Project, along with all the related SRS Project details, is deleted.

    Note: When you delete a SRS Project, the relationships with the associated Instrumented Functions, Logic Solvers, Protective Instrument Loops, and SIL Analyses are removed.