SIS Trip Reports

About SIS Trip Report

SIS Trip Reports are records that store details on events, which occurred on a safety instrumented system, such as a trip alarm. For example, if during a process, the gas pressure level increased to an unmanageable level and the safety instrumented system turned off the gas feed, you would create one SIS Trip Report to record the details of that trip alarm event.

When you create an SIS Trip Report, you will link it to a Logic Solver. When you create an SIS Trip Report Detail, you will select an Instrumented Function from among the ones that are linked to the Logic Solver. APM creates an SIS Trip Report Detail for each Instrumented Function that you have selected.

SIS Trip Report Details store details of the Instrumented Function with which it is associated. They also contain the decision that is made around the particular trip event, which is stored in the Action box. For example, you can specify a trip event as Dangerous or Safe.

Access an SIS Trip Report

Procedure

  1. Access the SIS Management Overview page.
  2. In the workspace, select the SIS Trip Reports tab.

    The SIS Trip Reports section appears, displaying a list of SIS Trip Reports.

  3. Select the SIS Trip Report that you want to access.
    Tip: You can also filter and search for the piece of test equipment by selecting in the upper-left corner of the workspace. The search results appear as you enter values.

    The datasheet for the SIS Trip Report appears.

  4. If needed, modify values in the available fields.
    Note: You cannot modify values if the SIS Trip Report is in the Complete state.
  5. In the upper-right corner of the datasheet, select .

    The changes made to the SIS Trip Report are saved.

Create an SIS Trip Report

Procedure

  1. Access the SIS Management Overview page.
  2. Select the SIS Trip Reports tab.

    The SIS Trip Reports section appears, displaying a list of SIS Trip Reports.

  3. In the upper-left corner of the section, select .

    A blank datasheet for the SIS Trip Report appears.

  4. Next to the Logic Solver ID box, select .

    The Search window appears.

  5. In the upper-right corner of the window, select .

    A list of Logic Solvers appears.

  6. Select the check box that corresponds to the Logic Solver that you want to select, and then in the lower-right corner of the window, select OK.

    The Logic Solver is selected.

  7. As needed, enter values in the other available fields.
  8. In the upper-right corner of the datasheet, select .

    The SIS Trip Report is created.

What To Do Next

Access an SIS Trip Report Detail

Procedure

  1. Access the SIS Trip Report for which you want to access an SIS Trip Report Detail.
  2. In the workspace, select the SIS Trip Reports Details tab.

    The SIS Trip Reports Details section appears, displaying a list of SIS Trip Reports Details linked to the SIS Trip Reports.

  3. Select the SIS Trip Report Detail that you want to access.

    The datasheet for the SIS Trip Report Details appears.

  4. If needed, modify values in the available fields.
    Note: You cannot modify values if the SIS Trip Report is in the Complete state.
  5. In the upper-right corner of the datasheet, select .

    The changes made to the SIS Trip Report Details are saved.

Create an SIS Trip Report Detail

Before You Begin

Procedure

  1. Access the SIS Trip Report for which you want to create an SIS Trip Report Detail.
  2. In the workspace, select the Trip Report Details tab.

    The SIS Trip Report Details section appears.

  3. In the upper-left corner of the section, select Add Trip Details.

    The Trip Details window appears, displaying a list of Instrumented Functions. These are the Instrumented Functions that are linked to the Logic Solver whose ID is populated in the Logic Solver ID field in the SIS Trip Report datasheet.

    Note: You can add SIS Trip Report Details only if the SIS Trip Report is in the Active state.
  4. Select the check box that corresponds to the Instrumented Function for which you want to create an SIS Trip Report Detail.
  5. In the lower-right corner of the window, select Add.

    The SIS Trip Report Detail is created.

  6. Select the SIS Trip Report Detail, and in the datasheet that appears, modify the details as needed, and select Save.

    The SIS Trip Report Detail is saved.

Delete an SIS Trip Report Details

About This Task

Procedure

  1. Access the SIS Trip Report for which you want to delete the SIS Trip Report Detail.
  2. In the workspace, select the SIS Trip Reports Details tab.

    The SIS Trip Reports Details section appears, displaying a list of SIS Trip Reports Details linked to the SIS Trip Reports.

  3. Select the check box that corresponds to the SIS Trip Report Detail that you want to delete.
  4. In the upper-right corner of the section, select .

    The SIS Trip Report Detail is deleted.

    Note: You cannot delete an SIS Trip Report Detail if the SIS Trip Report is in the Complete state.

Delete an SIS Trip Report

About This Task

Important: Deleting an SIS Trip Report also deletes the linked SIS Trip Report Details.

Procedure

  1. Access the SIS Management Overview page.
  2. In the workspace, select the SIS Trip Reports tab.

    The SIS Trip Reports section appears, displaying a list of SIS Trip Reports.

  3. Select the check box that corresponds to the SIS Trip Report that you want to delete.
  4. In the upper-right corner of the section, select .

    The SIS Trip Report, along with all the related SIS Trip Report Details, is deleted.