Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IServer Interface / GetSecurityGroupMembership Method


In This Topic
    GetSecurityGroupMembership Method
    In This Topic
    Retrieve the standard Historian security groups in which the currently authenticated user holds membership.
    Syntax
    Function GetSecurityGroupMembership() As HistorianGroupMembership
    HistorianGroupMembership GetSecurityGroupMembership()
    HistorianGroupMembership GetSecurityGroupMembership(); 

    Return Value

    The
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also