Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IServer Interface / GetCalcLibrary Method


In This Topic
    GetCalcLibrary Method
    In This Topic
    Retrieve the global set of calculations from a Historian server. The global calculation library enables a central repository and reuse of custom user calculation code across all calculation tags in a server.
    Syntax
    Function GetCalcLibrary() As Calculations
    Calculations GetCalcLibrary()
    Calculations^ GetCalcLibrary(); 

    Return Value

    A set of calculations.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also