Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IServer Interface / GetCurrentServerTime Method


In This Topic
    GetCurrentServerTime Method
    In This Topic
    Retrieve the current Historian server time expressed in UTC.
    Syntax
    Function GetCurrentServerTime() As System.Date
    System.DateTime GetCurrentServerTime()
    System.DateTime GetCurrentServerTime(); 

    Return Value

    The current server time.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also