Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / GetValue Method
An index value.


In This Topic
    GetValue Method
    In This Topic
    Return the data value at a specific index.
    Syntax
    Function GetValue( _
       ByVal index As System.Integer _
    ) As System.Object
    System.object GetValue( 
       System.int index
    )
    System.Object^ GetValue( 
       System.int index
    ) 

    Parameters

    index
    An index value.

    Return Value

    A data value.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also