Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / GetTime Method
An index value.


In This Topic
    GetTime Method (IDataSamples)
    In This Topic
    Return the data value time at a specific index.
    Syntax
    Function GetTime( _
       ByVal index As System.Integer _
    ) As System.Date
    System.DateTime GetTime( 
       System.int index
    )
    System.DateTime GetTime( 
       System.int index
    ) 

    Parameters

    index
    An index value.

    Return Value

    A data value time.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also