Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / Count Method


In This Topic
    Count Method (IDataSamples)
    In This Topic
    Return a count of data values.
    Syntax
    Function Count() As System.Integer
    System.int Count()
    System.int Count(); 

    Return Value

    Number of data values.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also