Uploading Packages

Upload applications to Predix Edge Technician Console so you can deploy them to the device.

Before you begin

You must create and package the application. If you are using the production version of Predix Edge OS, the application must be signed.

Procedure

  1. In the left navigation pane, click Applications Manager.
  2. In the Available Packages section, select Actions > Upload App.
  3. Click Choose File to browse for the package to upload.
    Note:
    Application packages must be packaged as gzip files and configurations as zip files. See the guidelines in Package Size Guidelines.
  4. (Optional) In Name, enter a name for the application.
    If you do not enter a name for the package, it defaults to the file name.
  5. Click Upload.
    You are returned to the Applications Manager page, where a success message appears at the top of the page and the uploaded package appears in the Available Packages list with a status of "Uploaded." You can now deploy the package to the device.