Applying Configurations

You can use the Applications Manager page in Predix Edge Technician Console to apply configurations to applications.

Procedure

  1. In the left navigation pane, click Applications Manager.
  2. In the Deployed Instances list, select the application to which to apply the configuration, then select Actions > Apply Config.
    Note:
    Configurations must be packaged as zip files, and do not have to be signed.
  3. In the Apply Configuration dialog box, click Choose File, select the configuration to apply, then click Upload & Apply.
    The application is stopped, and the configuration is applied. The status of the application changes as follows:
    1. Applying Configuration
    2. Starting
    3. Running