Deleting Packages

You can use the Applications Manager page to delete applications that are uploaded to Predix Edge Technician Console and packages that are deployed to the device.

Procedure

  1. In the left navigation pane, click Applications Manager.
  2. To delete packages that are uploaded to Predix Edge Technician Console (staged):
    1. In the Available Packages section, select the package to delete, then select Actions > Delete.
    2. In the Delete confirmation dialog, click Delete.
      The package is deleted from Predix Edge Technician Console and no longer appears in the Available Packages list.
      Note:
      This action does not delete deployed applications.
  3. To delete deployed applications:
    1. In the Deployed Instances section, select the package to delete, then select Actions > Delete.
      Note:
      Only applications with any of the following statuses can be deleted:
      • Running
      • Stopped
      • Error
    2. In the Delete Application dialog box, click Delete.
      The application status changes to "Deleting" and it is deleted from the device. After it is deleted, it no longer appears in the Deployed Instances list.