Repeater
A repeater layout displays a set of repeating objects.
The repeater functionality is available only in the flexbox card layout.
If you selected a repeater functionality for your flex layout, then configure these details:
Field Name | Description |
---|---|
Repeater Source | Select a query to retrieve data, which is displayed in the repeater. |
Multi Select | This property is used in combination with a map or a graph plug-in.
Select this check box if you want to insert a check box for
multi-selection. In the end application, a check box appears in each row of the repeater, allowing you to select which items should appear on the map or the graph. |
Checked | This property applies only if you enabled multi-selection check
boxes. Select this check box if you want multi-selection check boxes selected by default. When you open the end application, the check box that appears in each row of the repeater remains selected by default. |
Load | Select this check box if you want to add rows that appear by default in the repeater. |
Page Size | Enter the number of rows that should appear by default in the repeater. |
Paging Style | Choose from these options:
|