Coordinate Card
This layout offers an absolute layout design structure.
This is the default card layout when you start to design application pages. You can drag
and drop plug-in objects to an absolute position on the card. The end application
reflects the same as in the coordinate card page design.
Field Name | Description |
---|---|
Columns | The card occupies the specified number of columns on the page grid. |
Rows | The card occupies the specified number of rows on the page grid. |
Position X | Applies to the horizontal placement of the card on the page. When the
value is 0 , the card is placed on the left-most side of the
page. As you increase the value, the card moves away from the left side of the
page. |
Position Y | Applies to the vertical placement of the card on the page. When the value
is 0 , the card is placed at the top of the page. As you
increase the value, the card moves away from the top of the page. |
Layout Type | Choose from the following card layouts before starting to design your pages:
|
Style | Select these check boxes to format the objects:
|
Function | Layout functionalities:
|
scale Line Connector | Scale Line Connectors checkbox option: - We need to set 'Scale Line' connector option at card level and with this setting the line connector will work similar to %. All the other plugins that are connected using line connector needs to be in % when user is expecting to scale based on br*oswer page dynamic height and width changes. |
Show/Hide | Select +Add Conditions to create conditions to show or hide the card. |
Scroll bars will display for the card when card size is smaller than the plugin size.
Value display: - In new designer, Height & width will consider from widget properties not from the plugin manifest/properties (Height & Width).
Breadcrumb: - Breadcrumb combination with any other plugins used in coordinated layout , should follow the higher z-index properties than breadcrumb. ( Ex: Set the Breadcrumb z-index '0' and Alarm Card/Trend card should be z-index '1' )