Navigation Panel
This topic provides an overview of the navigation panel from Configuration Hub in the Operations Hub new layout.
Applications

1 | Creates a new application. |
2 | Imports application and pages. For more information on importing applications and pages, refer to the Operations Hub documentation. |
3 | Allows to perform the following actions:
|
4 | Opens a Column Chooser dialog. Select the check box
for the columns you want to show on the applications homepage. To hide columns,
clear the respective check box.
|
5 | Enter keywords to search for applications or pages. |
6 | Sorts columns in ascending or descending order. The status is indicated by the up/down arrow on each sortable column header. |
7 | Indicates whether the application is in a locked or unlocked state. |
8 | Allows to perform tasks on the selected application or page. You can
either:
Existing app/page names are quickly editable on the homepage itself. Note: Applications/pages created in the Operations Hub Classic
version cannot be modified in the new Operations Hub layout. Such
applications are marked as legacy apps. You can only preview
them. For more information on applications and pages, refer to the Operations Hub documentation. |
9 | Opens the end application. |
Plug-ins

1 | Enter keywords to search for plug-ins. |
2 | Expand System to view the system plug-ins
available in Operations Hub. See also Visuals Tab. |
3 | Expand Custom to view custom plug-ins. If you have saved any customized plug-ins, then they appear under custom plug-ins. |
4 | Reloads the plug-ins screen. |
For a high-level panel layout, see Panels Layout.