Display Panel
This topic provides an overview of the display panel in the Operations Hub new layout.
The display panel serves as the display area for working with applications and their pages within Operations Hub.
See Page Grid Details.
See Page Building Tools.
For a high-level panel layout, see Panels Layout.
Use Keyboard Shortcuts
UI Operation | Windows | Mac |
---|---|---|
Copy | Ctrl+C | Command+C |
Paste | Ctrl+V | Command+V |
Duplicate | Ctrl+D | Command+D |
Toggle line connector mode | L | L |
Toggle ruler | Ctrl+R | Command+R |
Redo | Ctrl+Y | Command+Y |
Undo | Ctrl+Z | Command+Z |
Perform Operations Using Multi-Selection
- Move all selected objects to a different position within the layout by dragging them or using arrow keys.
- Resize/Scale all selected objects collectively.
Move Objects Using Arrow Keys
- Select the object/s you want to move.
- Use left/right/up/down arrow key to move left/right/upward/downward on the
display area.
The object/s moves one pixel per key stroke.
- To continuously move the object/s in the associated direction, long press the
respective key and release when done.
On the Details panel, notice the Offset Left and Offset Right values are automatically adjusted to reflect the new position of the moved object/s.
Copy and Paste Objects on a Layout
You can duplicate object/s by copy/pasting them. Once copied, you can paste the duplicate in the desired location within the layout. In this way, you can create an identical copy of the object/s. This action allows you to easily create multiple instances of the same object without manually recreating it from scratch. Duplicates can be modified independently.