Update or Modify CIMPLICITY Node or Plug-in

About this task

If you want to modify the alias name for the CIMPLICITY plug-in or the node that is registered with Configuration Hub, you can do that using the node manager in Configuration Hub.

To update or modify the plug-in, do the following:

Procedure

  1. In the machine that has Configuration Hub installed, in the desktop, double-click .
    Alternatively, in the CIMPLICITY node machine, you can open Configuration Hub from the Workbench.
    The Proficy Authentication login page appears.
  2. Log in using ch_admin as username and your Proficy Authentication secret as password.
    After a successful authentication, the Configuration Hub page appears.

    By default, in the NAVIGATION pane, the Proficy Authentication and Administration plug-in appear.

  3. In the NAVIGATION pane, select Administration, and then expand it.
    Node Manager and License Server appear.

  4. Select Node Manager.
    The Node Manager-Administration panel appears.
  5. To modify a plug-in display name, expand the node, and then select the plug-in.
  6. In the right-side pane, in the PLUG-IN details, you can enter a new display name for the plug-in.
    The display name of the plug-in gets updated.

    Alternatively, you can right-click the node, and then select Manage Plug-ins.

    The Manage Plug-ins window appears, allowing you to select the plug-in in the node and modify the plug-in's display name.
    1. Select the plug-in as needed.
    2. In the Plugin Display Name column, modify the name of the plug-in.
    3. Select Update.

      The plug-in name gets modified.

  7. To modify a node's display name, select the node.
  8. In the right-side pane, in the NODE MANAGER details, you can enter a new display name for the node.
    The display name of the node gets updated.