Start and Stop a CIMPLICITY Project
About this task
Note: If you have set the CIM_SSL_STRICTPOLICY parameter to Y
(recommended), it is important that the primary server trusts the secondary server's SSL
certificate, and vice versa.
To start a project, perform the following:
Procedure
-
In the machine that has Configuration Hub installed, in the desktop, double-click
.
Alternatively, in the CIMPLICITY node machine, you can open Configuration Hub from the Workbench.The Proficy Authentication login page appears. -
In the NAVIGATION pane, select and expand the required
node.
All the associate plug-in and its projects are listed.
-
Select a project, and then select the ellipsis (...) to the right of your entry in
the Actions column.
Alternatively, you can right-click on the required project and select the actions as needed.A popup menu appears.
-
Select an action as needed.
The below table explains the available options:If you select Stop, a confirmation popup appears. Select Yes to stop the project.
Option Description Start Select this to start a stopped project. Stop Select this to stop a running project. Start Primary and Secondary Select this to start a stopped project in both primary and secondary servers. Start Primary Select this to start a stopped project in primary server only. Start Secondary Select this to start a stopped project in secondary server only. Stop Primary and Secondary Select this to stop a running project in both primary and secondary servers. Stop Primary Select this to stop a running project in primary server only. Stop Secondary Select this to stop a running project in secondary server only.