Register the CIMPLICITY Node with Proficy Authentication
Before you begin
About this task
Procedure
-
From the desktop, open the Node Manager Configuration
utility as an administrator.
The Node Manager Configuration utility appears.Node manager details on this host- This section displays the CIMPLICITY node's hostname and port number. Make a note of it as you will need these details while you add the node in Configuration Hub.
Proficy Authentication- This is the section where you must enter the details of the Proficy Authentication server that the CIMPLICITY node will use, as well as the one Configuration Hub is using. This will enable Configuration Hub to trust the CIMPLICITY node when you add it.
-
In the Proficy Authentication section, enter the following details:
Field Description Host Name The hostname of the Proficy Authentication server to which you want to connect the CIMPLICITY node.
Port The port number of the Proficy Authentication server. By default, it is 443. Client ID The client ID of the Proficy Authentication server, provided during the Proficy Authentication server installation. Client Secret The client secret of the Proficy Authentication server, provided during the Proficy Authentication server installation. If the root certificate of the Proficy Authentication server is not trusted, then click not trusted
, the Certificate Details page appears. Select Trust to trust the root certificate.
-
After you enter the needed details, select Configure.
A success message appears stating that the Proficy Authentication was commissioned with Node Manager.
What to do next
Add the CIMPLICITY Node and Register the Plug-in with Configuration Hub