CIMPLICITY Plug-in Registration Use Cases
The following use cases provide detailed information on the different registration methods. You can use these uses cases as a reference to decide on the registration method.
First time Install: CIMPLICITY, Common components like Configuration Hub, and Proficy Authentication (Version 2024 or higher)
Scenario | Tasks to Perform |
---|---|
Common components installed before CIMPLICITY. | Perform install time registration during the
CIMPLICITY installation. Note: If you skip providing
Configuration Hub and Proficy Authentication details during the installation,
then perform central registration
after installing CIMPLICITY. |
Common components installed after CIMPLICITY installation. | Perform central registration after installing CIMPLICITY. |
CIMPLICITY Upgrade from Version 2023 to 2024 or higher version
Important: To upgrade your previous versions of
CIMPLICITY, you must uninstall the previous version first and then install the latest
CIMPLICITY, that is 2024 or later. If you have registered a CIMPLICITY plug-in in
Configuration Hub, you must first unregister the plug-in and then uninstall the existing
version of CIMPLICITY. For more information on how to unregister a plug-in from
Configuration Hub, refer to the Unregister CIMPLICITY Plug-in from Configuration Hub
section in the CIMPLICITY 2023 online documentation.
Scenario | Tasks to Perform |
---|---|
Common components already upgraded to version 2024 or higher. | Perform install time registration during the
CIMPLICITY upgrade, that is while installing CIMPLICITY 2024, after uninstalling
the previous version of CIMPLICITY. Note: If you skip
providing Configuration Hub and Proficy Authentication details during the
upgrade, then perform central registration method after the installing the latest
CIMPLICITY. |
Common components are installed later with version 2024 or higher. | Perform central registration after installing CIMPLICITY. |
Common components installed but not upgraded to version 2024 or higher. |
Important: Upgrade common components to version
2024 or higher.
|
CIMPLICITY Unregistration
Scenario | Tasks to Perform |
---|---|
CIMPLICITY registered with version 2024 common components or higher. | Unregister CIMPLICITY centrally from Configuration Hub. Unregister CIMPLICITY plugin. |
CIMPLICITY of version 2023 (registered conventionally) to common components of version 2024 or higher. | Unregister CIMPLICITY conventionally. Kindly refer to the CIMPLICITY Plug-in Registration with Configuration Hub section in the CIMPLICITY 2023 online documentation |
Pre-2024 CIMPLICITY Registration
Scenario | Tasks to Perform |
---|---|
Older version of CIMPLICITY registration and unregistration with common components of version 2024 or higher. | Follow the conventional process for registration and unregistration. Kindly refer to the CIMPLICITY Plug-in Registration with Configuration Hub section in the CIMPLICITY 2023 online documentation. |
Migration of Common Components (Version 2024 or later) Post-Registration
Scenario | Tasks to Perform |
---|---|
If you migrate to a new Proficy Authentication server. |
|
If you migrate to a new Configuration Hub server. |
|
If you migrate both the new Configuration Hub server and the Proficy Authentication server. |
|