Start and end a test debugging session

You can troubleshoot problems that may be occurring in a workflow by tracking the flow of logic in a workflow.

Before you begin

Note:
A resource must already have been added in order to select it from this list.

Procedure

  1. In the navigator, click Workflow.
  2. In the resource list, select the workflow that you want to work with. If no workflow exists, create a new workflow.
  3. In the resource type list, select a resource.
  4. In the Displays panel, click Workflow Management > Workflow Editor.
  5. Click the Test/Debug tab.
  6. To start a test debugging session, click Test.
  7. To see the workflow in a debugging session, click the Workflow Editor tab.
  8. To end a test debugging session, click the:
    • Test/Debug tab, and then click Stop Testing, or
    • Stop Testing button on the Debugger Control Bar.
  9. To discontinue the debugging session, click the Test/Debug tab.
  10. Optionally, to remove the debugger, click Detach.