Configure a Create Event activity

Before you begin

Note:
Activities can be inserted at both the workflow and subprocess levels.

Procedure

  1. In the navigator, click Workflow > Workflows.
  2. In the resource list, select the workflow that you want to work with. If no workflow exists, create a new workflow.
  3. In the Displays panel, click Workflow Management > Workflow Editor.
  4. Click the Workflow Editor tab.
  5. Drag and drop a Local Subprocess into the workflow and double-click it, or double-click an existing subprocess.
  6. On the activity configuration panel, click Configure Event next to Conditional Event.
    The Configure Conditional Event dialog box appears.
  7. Create a condition event.
    Note:
    For more information, see Condition Events.
  8. Click OK, and then click Save.