Add an activity to a fault handler activity

Before you begin

Note:
Activities can be inserted at both the workflow and subprocess levels.

Procedure

  1. In the Navigator, click Workflow > Workflow.
  2. In the Workflows list, select the resource you want to work with
    Note:
    A resource must already have been added in order to select it from this list. For more information, see .
  3. In the Displays panel, click Workflow Management > Workflow Editor.
  4. Click the Workflow Editor tab.
  5. Insert an activity:
    • At the workflow level:
      • From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
        Note:
        Activities can exist only between the presubprocess and postsubprocess.
    • At the subprocess level:
      • Double-click the local subprocess you want to add the activity to.
      • From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
  6. Double-click the process step you want to work with.
  7. On the activity configuration panel, click Show fault handlers for this activity next to View.
  8. In the workspace, click Click here to add a fault handler.
  9. Double-click the fault handler activity you want to add an activity to.
  10. Insert an activity.
  11. To return to the process step, click the link in the breadcrumbs.