Supercharge your Proficy solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Explore our Proficy 2025 releases!
You can use the REST APIs to interact with the Workflow application over the Internet.
You can create a signature record based on a provided definition. A record must be created before it can be signed.
The signature record can be signed once for the performer, and, if required, a second time for the verifier. When all signatures are complete, the record is closed. To sign an existing signature record, you use the signature ID that is returned from the creation request.
You can retrieve an in-progress or completed signature record.
You can cancel an in-progress signature record.
If a REST operation fails, additional information about the error is available from both the response Error-Code header and the response body.
All equipment methods use the same base URL.