Material Model Tables
In the Material model, there is no measurable data; most of the facts are relations.
The following table describes the reporting database tables and their descriptions.
Table | Description |
---|---|
Dim_Material | Material definitions. |
Dim_MaterialClass | Material class definitions. |
Fact_MaterialActual | Material actuals. |
Fact_PropertiesOfMaterial | Material property configuration, including both class properties and instance properties. |
Fact_ClassesOfMaterial | Material class and Material definition association. |
The following diagram illustrates the relationship between the Material model tables: