Manual Inputs

The Inputs section displays information that requires operator interaction for a task step, such as a manual start or a form submission.If a task is preconfigured to wait for an operator to start it, you must manually start a task step to progress the workflow.

If configured, you can view completed or acquired task forms. When a completed task step is selected, the last submitted form for that task step is shown. If an acquired task step is selected, the currently executing form is shown.

InputValueDescription
Manual StartPreconfiguredRequires operator interaction. The Start button advances the workflow.
Form inputUser-defined; PreconfiguredRequires operator interaction. Complete the form and submit it to advance the workflow. If applicable, cancel the form to advance the workflow; however, the Cancel button is available only if the user has permission to do so. You can also use the Status Message to get more information about your form.
Tip:
In the Mobile-sized Task List, you can use the arrow next to the Form button to display a selection of all available forms, both running and completed, and then select a form from the list. When there are no more task steps to perform, you will be notified and the Start Task button becomes available.
E-signatureUser-defined; PreconfiguredRequires operator interaction. A form may need to be signed electronically before it is submitted. Sign the form and submit it to advance the workflow.
Note:
This feature is not available on the Mobile-sized Task List. You will receive an error message and the form will not load if you try to open a form that requires an e-signature.