Load
The load step is the first step in a workflow cycle. It is used to perform a one-time only setup for the workflow instance.
The load process is a good starting point to add initial data common setup procedures inherent to your process. It is also a good starting point from which to facilitate the completion of other subprocesses located within the workflow instance. By using the load step in this manner, you can ensure that the necessary steps for the process are enabled and executed.
If the workflow is set on a continuous loop, this step only runs once.