Jump
You can skip to, or jump to, a particular task in the Task List.
How Jump Works
Cancelled Task Steps
Using this feature, an operator can jump back to the beginning of a task or set of task steps to do a completed or cancelled task step again. A task then resumes execution from the jump point. For example, if step 1 and step 2 have completed, and step 3 is running, and you then jump back to step 1, then steps 1, 2, and 3 execute.
Skipped Task State
If a task step is selected in the later portion of a task, all uncompleted steps previous to the selected step are skipped and their status changes to Skipped.
User Interface