End Task Activity
When designing a workflow, you can use this activity to cancel or complete a task that is currently executing in a running workflow.
Note:
Continuously looping workflows are not affected by this activity.
Attribute | Value | Description |
---|---|---|
Complete Task | User-defined; Boolean | Select this option to ensure that the workflow cancels all executing activities and transitions to completion. The postsubprocess and postprocess activities finish as expected before the task is completed. |
Cancel Task | User-defined; Boolean | Select this option to ensure that the workflow cancels all executing activities and transitions to a cancelled state. When you select this option, the Cancel Reason appears. |
Cancel Reason | User-defined; String |
Associated with Cancel Task. Specifies a reason that the task was cancelled in order to provide more data on the operation. This value can be configured using a literal value, expression, or bind. If no information is entered into this field, the default reason is Cancelled by system. . |