Computer Configuration Summary

The Details tab of the Computer Editor provides summary information about the selected computer's configuration.

Edit Description

You can change the description of this resource.
AttributeValueDescription
DescriptionUser-defined up to 255 charactersProvides more information about a resource that a user may find helpful.

Details Tab

The following table describes the available options.

AttributeValueDescription
Override Default ConfigurationN/ASelect this check box to indicate that the settings for the selected computer will override the global default configuration and use startup options configured specifically for it. Clear this check box to indicate that the selected computer will use the global default configuration.
Auto LoginN/ADisplays whether the computer is configured for automatic login for any users.
Auto LogoutN/ADisplays whether the computer is configured for automatic logout for any users.
Lockdown modeN/ADisplays whether the lockdown mode is configured on the computer.

When lockdown is enabled, you cannot access anything outside of the Workflow client, but may log in or log out. When lockdown is disabled, you can access other programs, minimize the client, and so on.

Default Startup OptionsN/ADisplays the startup options that are configured on the computer.