Client Configuration

The Client Configuration tab on the Computer Editor allows you to enable or disable lockdown mode, to define the default startup options for a specific workstation, and to link a piece of equipment to a specific workstation.

On the Default Computer Editor, the Client Configuration tab allows you to define the default startup options for a all of the computers in your system or a subset of those computers.
Note:
This tab is available in the Computer Editor only if the selected computer is configured to override the global configuration settings.

An information message is posted in the Feedback Zone any time a change is detected in the configuration settings of the functions.

Lockdown Mode

The following table describes the available options.

AttributeValueDescription
Enable Lockdown modeUser-definedSelect this check box to keep Workflow displayed at all times.

When lockdown is enabled, you cannot access anything outside of the Workflow client, but may log in or log out. When lockdown is disabled, you can access other programs, minimize the client, and so on.

Equipment Link

The following table describes the available options.

AttributeValueDescription
Link to EquipmentUser-definedClick to open the Universal Browser to select an equipment location to associate with this computer.
Clear Equipment LinkN/AClick to clear the equipment location association from the selected computer.

Default Startup Options

The following table describes the available options.

AttributeValueDescription
Layout Configuration: Show Solution PaneUser-definedSelect this check box to specify whether the Solution Panel is displayed on the selected workstation when Workflow starts up.
Layout Configuration: Show navigatorUser-definedSelect this check box to specify whether the navigator is displayed on the selected workstation when Workflow starts up.
Startup Object: Navigate Users on LoginUser-definedSelect this check box to enable the Change Startup Object link.
Startup Object: Change Startup ObjectIser-definedClick to open the Universal Browser to select the object that will be displayed on the selected workstation when Workflow starts up.
Default Startup Options: Users will be started in a specific solution/displayUser-definedSelect this check box to enable the Change Startup Solution link.
Default Startup Options: Change Startup SolutionUser-definedClick to open the Universal Browser to select the solution and display that will be displayed on the selected workstation when Workflow starts up.