Set Up Data Source Servers

You set the data source servers used to populate data in your model.

You can set up multiple Historian servers.
  1. In the Administration environment, select Set Up and then Server.
    The Server Details Management screen appears.
  2. To add each data source, do the following:
    1. Select + above the table.
    2. In SystemAlias, enter the alias for the server.
    3. In SystemType, select the data source type from where data originates.
    4. In SystemName, specify one of the following:
      • For iFIX, enter the logical node name.
      • For Historian, enter the server name.
      • For CIMPLICITY, copy the Uniform Resource Name (URN) from the CIMPLICITY Project Properties screen or from the .csv file containing the project server and namespace information exported from CIMPLICITY and paste it in to this field.
      • For Workflow, enter the server name. Workflow requires a refresh rate between 1 and 30 seconds to poll the server for new and updated tasks. The default is 5 seconds. You can only set up one Workflow server.
  3. Select Save.