Bind Mimics to Assets
Asset objects can reuse the mimics that you bind to their object types. This enables Web HMI navigation to display the correct mimic in the HMI card in the context of the model.
- In the Administration environment, navigate to .
- Select Types.
- Select the asset object type in the left panel.
- In the Mimic field on the Details tab, select a mimic from the drop-down list to associate with this asset object type.
- Select Save.
- Select Mimic Card for the selected asset object type.The Mimic Fields display the animation sources within the mimic. For example, @Flow@ and @OpenClose@ are fields on a mimic for displaying data for the Suction Value asset object type.
- To bind a mimic field with a data variable in the model:
- Select Mimic Binding to choose a variable from the drop-down list for each mimic field.
- To let Web HMI automatically perform the binding by matching the data variable and mimic field names, select Autobind. For example, a
TPump
asset object type with a variable namedFlow
automatically binds with a picture representing a pump with the @Flow@ animation.
Note: If you add or remove properties in an asset object after binding a mimic to it, check the mimic field bindings to ensure they are correct. - Repeat these steps as needed to bind each mimic to an asset object type.
- Select Save.