Change the Property Groups or Values of a Work Order

Before you begin

If you do not have the permission to perform this task, a message appears, stating the same. If that happens, request your administrator to provide the permission using Security.

About this task

You can add a property group or modify the values of properties in a work order only if the corresponding operations are ready or not started.

Procedure

  1. Access the work order that you want to modify.
  2. In the upper-right corner of the page, select , and then select Edit workorder.
    The Edit <work order> page appears, displaying a list of operations in the work order.
  3. Select Properties.
    The Properties workspace appears, displaying a list of property groups assigned to the route appears.
  4. If you want to enter or modify the value of a property:
    1. Expand the group that contains the property whose value you want to enter or modify.
      A list of properties in the group appears.
    2. Enter or modify the value in the VALUE column for each property for which you want to provide a value. The following conditions apply when you provide a value for a property:
      • If a property has been specified as mandatory in the Property Definition application, you must provide a value for the property.
      • The value must be of the same data type as specified in the DATA TYPE column.
  5. If you want to assign a property group to an operation or all operations in the work order:
    1. If you want to assign a property group to an operation, select the operation. If you want to assign a property group to all operations in the work order, select ALL OPERATIONS.
      Note: You can select an operation only if it is not started. You can select ALL OPERATIONS only if at least one of the operations is not started.
    2. Select .
      The Assign Property Group(s) window appears, displaying the property groups that have group definitions.
    3. Select the check boxes corresponding to the property groups that you want to assign.
      Tip: If you want to assign all the property groups, select the check box in the heading.
    4. Select Assign.
  6. Select Save.
    The changes made to the work order are saved.