If you do not have the permission to perform this task, a message appears, stating the same. If that happens, request your administrator to provide the permission using Security.
About this task
You can change the BOM assignment of an operation only if the operation is not started.
In the upper-right corner of the page, select , and then select Edit workorder.
The Edit <work order name> page appears, displaying a list of operations in the work order.
Select BOM.
The BOM workspace appears, displaying a list of BOM items in the PRODUCT DESCRIPTION column. The SEQUENCE, PRODUCT CODE, QT PER, and UOM columns are populated with the sequence number of the BOM item, the product code, the quantity needed per operation, and the units of measure of the associated BOM formulation, respectively. You cannot modify these values.
In the OPERATION column, select the operation that you want to link to the BOM items. You can only select an operation that is not started. If the behavior of an operation is set to Non Clocking, the operation does not appear in the list.