Enterprise Edition Web Client Requirements

Before you begin

Ensure that you have completed following tasks :

System Requirements

Ensure that your computer meets the system requirements as described in the following table.
Item Version
Operating system Redhat 7.8 and 8.2 or Ubuntu 18.x
Note: Ubuntu is not supported in a production environment.
Docker
Web browsers Chrome 85.0 or later, with minimum resolution 1366x768.
Devices:
  • iPad: Safari v13.1+, Chrome 85.0 or later with resolution 2048x1536
  • HP tablet: Chrome 85.0 or later , with minimum resolution 1920x1280
    Note: Devices supports only Unit Operations,Work Queue, and Non Conformance applications.
    .
Couch DB server CouchDB version 2.3.1 and later installed and configured on a Windows machine. GE also supports CouchDB 3.2.2.
Note: For more information on configuring CouchDB, refer to Configuring Apache CouchDB Settings.
Hard drive 100 GB (minimum)
Note: However, you may need more disk space based on your production data.
Processor 2.4 GHz clock-speed Intel Core i3, i5, or i7 CPU or equivalent AMD Phenom CPU
Note: For better performance, it is recommended to use an octa core (8-cores).
Memory 32 GB (recommended)
Note:
  • You can combine the Installer node, Plant Applications Web Client node, and the Local Docker Registry node into a single Linux server, especially if you want to upgrade to Plant Applications 8.2.
  • If you are using controller and performing a remote upgrade of 8.0 SIM2, then you must uninstall the docker-py module on the Enterprise Edition Web Client node before starting the upgrade process.

Port Requirements

Ensure that the ports described in the following table are opened before you install Plant Applications Web Client.
Port Description
15672 The default port for the RabbitMQ Message bridge required to communicate with the Plant Applications server for retrieving data updates.
1433 The default port for the Microsoft SQL server.
9093 The default port for Kafka.
2185 The default port for ZooKeeper.
6984 The default port for CouchDB.
5059 The default port for Web Applications