About this task
For an operation that requires clocking on, if the completed quantity of a serial/lot is equal to the planned quantity for the work order, the operation is automatically marked complete for the serial/lot. If, however, the operation does not require clocking on, and if you have performed the operation on the serial/lot, you must mark the operation complete. It is then removed from the list in the Work Queue page. After all the operations are marked complete for all the serials/lots in a work order, the work order is marked complete in Plant Applications. You can view the completion status of the work order in Work Order Manager.
Procedure
- In the row containing the operation that you want to mark complete, select
.
Note: The

button appears only if the completed quantity of the serial/lot equals the planned quantity for the work order or if the operation does not require clocking on.
The Select Serial/Lot number(s) to Complete window appears, displaying a list of serials/lots in the work order that are clocked on by you for the operation. If, however, the operation does not require clocking on, a list of all the serials/lots in the work order appears.
- Select the check boxes corresponding to the serials/lots for which you want to mark the operation complete, and then select Complete.
Tip:
- If you want to mark the operation complete for all the serials/lots in the list, select the check box in the heading row of the table.
- You can search for a serial/lot by entering a value in the search box or by scanning for the bar code using the
icon, and then selecting the check boxes from the filtered list that appears.
Note: By default, the EQUIPMENT box is populated with the piece of equipment assigned for the operation. If required, you can select a different piece of equipment.
Results
If the operation is marked complete for all the serials/lots in the work order, the operation no longer appears in the Queue page. It appears in the By Work Order page until all the operations in the work order are complete.