Search for an Operation
Procedure
- In the main navigation bar, select
.
A window containing a list of search options appears. - Provide values in any of the available boxes as described in the following table.
Box Description SERIAL/LOT Enter a serial/lot number to access the associated operations. WORK ORDER Enter a work order number to access the associated operations. MATERIAL FAMILY Select the material family of the serial/lot. MATERIAL Select the material of the serial/lot. The options in this box are filtered based on the value in the MATERIAL FAMILY box. EQUIPMENT Select the machine that is used to perform the operation. STATUS Select the status of the operation. Clocked On Select the check box to access the operations that are clocked on by you. Tip: To search for an operation using a barcode, selectfor an option, and scan for the barcode specific to the option.
- Use your device's front camera only for Barcode/QR code scanning. The application supports one-dimensional (Aztec, Data Matrix, MaxiCode, PDF417, UPC-A, UPC-E, UPC/EAN Extension) and two-dimensional (Codabar, Code 39, Code 93, Code 128, EAN-8, EAN-13, ITF, QR Code, RSS 14, RSS Expanded) types of standard codes.
- In iPad, you can use
only in the Safari browser.
- Select
for a field to filter the operations.
Results
Tip: To clear the results and perform new search, select Clear Results.