Access BOM Items

About this task

A Bill of Material (BOM) contains BOM formulations that define a list of items and the quantity of each BOM item needed to produce a product. BOM items are defined and associated with BOM formulations in Plant Applications. Using Plant Applications Web Client, you can manage BOM items as follows:

  1. In Route Editor, you can link BOM formulations to a route, and then link BOM items to operations.
  2. In Work Queue and Unit Operations, you can specify the consumption of BOM items for each serial/lot.
  3. In Work Order Manager, you can view the required and consumed quantity of each BOM item for each serial/lot.

Procedure

  1. Access the work order whose BOM items you want to view.
    The page for the work order appears, displaying the Current Status section. The All Serials/Lots section displays a list of serials/lots in the work order, along with the status of each serial/lot.
  2. In the left pane, select the serial/lot for which you want to access the BOM items.
  3. Select BOM.
    A list of BOM items associated with the serial/lot appears. The following table provides information on the columns in the table.
    Note: The list of BOM items appears only if you select a serial/lot in the left pane. If All Serials/Lots is selected, the list of BOM items does not appear.
    Tip: You can search for a BOM item by entering the part number in the Search part here box or by scanning the bar code of the part number.
    ColumnDescription
    ORDERThe order in which the BOM items may be consumed.
    PART#The part number of the BOM item.
    DESCRIPTIONThe description of the BOM item.
    REQ QTYThe required quantity of consumption of the BOM item to perform the operation on the serial/lot.
    CONSUMED QTYThe cumulative consumed quantity of the BOM item.
    UOMThe units of measure of the BOM item.
    SERIAL/LOT#The serial/lot for which the BOM item has been used.