Modify the Continue-to-Process (CTP) Disposition Method
About this task
- The operation until which the serial/lot can be processed.
- The disposition method, which can be changed from CTP to any of the other disposition methods such as, Clear, Scrap, Rework or Use as is.
- The disposition action reasons.
- Additional information related to the disposition.
The following conditions apply when you modify a CTP disposition method:
- When the you select the CTP disposition method for a plan, all the defects in the plan are moved to the Active status.
- You can modify the CTP disposition method only if all the defects in the plan are in the Active status. If at least one of the serials/lots completes the CTP operation (that is, the defect moves to the Submitted status), you cannot modify the CTP disposition method.
- You can dispose the plan if all the serials/lots complete the CTP operation (that is, all the defects are moved to the Submitted status).
Procedure
Results
Disposition Type | Result for a Serialized Product | Result for a Non-Serialized Product |
---|---|---|
Clear |
| If this is the only disposition method specified for the lot:
|
Continue to process (CTP) |
|
|
Use as is |
| If the disposition methods for the lot do not include MRB, Rework, or CTP:
|
Scrap |
| If the disposition methods for the lot do not include MRB, Rework, or CTP:
|
Rework |
|
|
MRB |
|
|