Clear | If this is the only disposition method specified for the lot:- The status of the defect is set to Not a Defect, indicated by
. - The hold on the serial/lot is released.
If the disposition methods also include Use as is or Scrap (but do not include MRB, Continue to Process, or Rework): - The status of the defect is set to Closed, indicated by
. - The hold on the serial/lot is released.
If the disposition methods also include MRB, CTP, or Rework:- The status of the defect is Active, indicated by
. When the defect is in the Active status, the hold on the serial/lot is released. - In the case of CTP or Rework, when the operation specified in the USE UNTIL/REWORK OPERATION box is reached, the serial/lot will be placed on hold. The defect status is changed to Planned, indicated by
.
|
Continue to process (CTP) |
- The status of the defect is Active, indicated by
. When the defect is in the Active status, the hold on the serial/lot is released. - When the operation specified in the USE UNTIL/REWORK OPERATION box is reached, the serial/lot will be placed on hold. The defect status is changed to Planned, indicated by
.
|
Use as is | If the disposition methods for the lot do not include MRB, Rework, or CTP:- The status of the defect is set to Closed, indicated by
. - The hold on the serial/lot is released.
If the disposition methods for the lot include MRB, Rework, or CTP:- The status of the defect is Active, indicated by
. When the defect is in the Active status, the hold on the serial/lot is released. - In the case of Rework or CTP, when the operation specified in the USE UNTIL/REWORK OPERATION box is reached, the serial/lot is placed on hold. The defect status is changed to Planned, indicated by
.
|
Scrap | If the disposition methods for the lot do not include MRB, Rework, or CTP:- The status of the defect is set to Closed, indicated by
. - The hold on the serial/lot is released.
If the disposition methods for the lot include MRB, Rework, or CTP:- The status of the defect is Active, indicated by
. When the defect is in the Active status, the current serial/lot will be released from hold. - In the case of Rework or CTP, when the operation specified in the USE UNTIL/REWORK OPERATION box is reached, the serial/lot will be placed on hold. The defect status is changed to Planned, indicated by
.
|
Rework |
- The status of the defect is set to Active, indicated by
. After completion of the rework operation, the status is changed to Planned, indicated by . - The serial/lot continues to be on hold. The hold is released after the completion of rework.
|
MRB |
- The status of the defect is set to Active, indicated by
. - The serial/lot continues to be on hold.
|