In the list of downtime events, select the check box of the target downtime events to copy the faults and reasons.
Note: The selected downtime events and equipment must belong to the same location.
The button is enabled for the cleared rows.
Select for the source downtime event row from which you want to copy the faults and/or reasons.
Note: Depending on the configuration set for the CopyPaste Type site parameter in the Plant Applications Administrator, one of the following options is displayed for the downtime event:
Reason only
Fault only
Both fault and reason
Select OK to confirm that you want to copy the faults and/or reasons for the selected downtime events.
Results
The target downtime events now have the same faults and reasons as the source downtime event.